Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello
I am rebuiding the sfh_OMAP-L138.exe for my board(DDR2+NOR FLASH 16BIT+25MHZ+UART1),but it only can be used on TI'board(EVM mDDR+SPI FLASH+24MHZ+UART2).
On my board will appear the following error.
E:\>sfh_OMAP-L138.exe -erase -flashType NOR
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2012, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
Platform is Windows.
[TYPE] Global erase
[TARGET] OMAPL138
[DEVICE] NOR
[NOR Block] 0
Attempting to connect to device COM1...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 10792-Byte section to address 0x80000000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): I/O Error in read!
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): I/O Error in read!
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): I/O Error in read!
what's caused that.??????????????????
waiting for ......................................
Thanks!!!!!