This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x mksd-ti814x.sh failed

Good afternoon

 

If got a problem:

 

I try to build the sd-card for u-boot. All compiles seems to be done correct. After building 2-stage u-boot and kernel i want to build the sd-card. I call

 

"sudo ./mksd-ti814x.sh /dev/sdb MLO u-boot.bin uImage nfs.tar.gz" at the folder where all this files are located.

 

For that I get the following output

1024+0 Datensätze ein
1024+0 Datensätze aus
1048576 Bytes (1,0 MB) kopiert, 2,70078 s, 388 kB/s
Festplatte /dev/sdb enthält keine gültige Partitionstabelle  //no valid partition table
DISK SIZE - bytes
(standard_in) 1: syntax error
CYLINDERS -
sfdisk (util-linux-ng 2.17.2)

 

to prepare the partition table I used gparted and built all possible partition tables. The disk is umount before starting mksd-ti814x.sh.

 

Any idea wht is wrong?

  • Hi Oliver,

    Script will do partitioning the card as well as copying all the files.

    I think problem with your card/host machine (if you are using ubuntu with virtualBox, I have seen some times this issue), can you please try with some other card/machine.

    Regards

    AnilKumar

    Please mark this Forum post as answered via the Verify Answer button below if it helps answer your question.  Thanks!