This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 MDIO Peripheral Register

Hi,

My original board have two phy (VITTESE VSC8641) that the two connected to DM8168.

It shows "0x0003" at MDIO Peripheral Register -> ALIVE (0x4A10 0808) .

But another board have two phy (REALTEK RTL8211) that the two connected to DM8168.

It shows "0x0007" at MDIO Peripheral Register -> ALIVE (0x4A10 0808) .


Is the same configuration, but the value is different Why?

Regards,

Shinji