This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Testing DMAI applications



Hi,

   In the article  "GSG: DVSDK for WinCE - Running the Demos ", The section "Testing DMAI applications",

  What is the meaning of the sentence--"Issue the desired commands shown in the following
subsections at the target control prompts provided in Visual Studio 2005 Professional Edition (with Windows
Embedded CE 6.0 R2/R3 with Platform Builder support installed)"

  • The commands described in the manual needs to be typed in the special command prompt provided by Platform Builder inside Visual Studio 2005. If you have installed Windows Embedded CE 6 on your computer and built the BSP from Platform Builder, you can then connect to your board using KITL over Ethernet/USB connection. Once your board has booted up and connected to Visual Studio/Platform Builder through KITL, type "Alt+1" in Visual Studio to make the "Target control" window appear. You can then directly type the DMAI test commands in this window.