Hi,
I had a general question on the performance when using descriptors and the associated entries in link ram. The link ram can handle 16000 entries only over 8 cores. I need probably of the order of double that i.e. 32K entries over 8 cores and so will have 16K entries in an external link ram stored in DDR3 together with all the 32K descriptors and the buffers that they point to all being stored in DDR3.
My question is what the is the performance tradeoff (i.e. how much loss in performance) in making use of the external link RAM in DDR3 over shared RAM over internal link RAM. Also what is the performance tradeoff with descriptors and buffers being stored in DDR3 as opposed to shared RAM or individual core RAM.
Thanks, Aamir