This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About connecting between AM3359 and TLK110 for EtherCAT.

Guru 10570 points

Other Parts Discussed in Thread: TLK110, AM3359


Hello,
I am referencing schematic which connecting between AM3359 and TLK110 on ICE and IDK.
AM335x datasheet describes that on ZCZ BALL PRUSS/MII0 Signals are :
(SPRS717B P63: Table 2-32. PRU Subsystem/MII0 Signals Description)

 - pr1_mii0_col [T10]
 - pr1_mii0_crs [T13, V5]
 - pr1_mii0_rxd0 [U4]
 - pr1_mii0_rxd1 [U3]
 - pr1_mii0_rxd2 [U2]
 - pr1_mii0_rxd3 [U1]
 - pr1_mii0_rxdv [T5]
 - pr1_mii0_rxer [V3]
 - pr1_mii0_rxlink [V2]
 - pr1_mii0_txd0 [T2, V13]
 - pr1_mii0_txd1 [R12, T1]
 - pr1_mii0_txd2 [R4, T12]
 - pr1_mii0_txd3 [R3, U12]
 - pr1_mii0_txen [R2, T11]
 - pr1_mii_mr0_clk [V4]
 - pr1_mii_mt0_clk [R1, U10]


But, Both ICE and IDK have not used U1, U2, U3, U4 signals.
Although instead it have used V5, U5, R5, R6, I think they do not have pr1_mii0_xxx function.


Should I use V5, U5, R5, R6?
Can they operate as MII I/F?

Best regards,
RY