This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SBOOT debugging using CCS v3.3.82.13



Hi,

We have the CCS v3.3.82.13

Processor: OMAP 5910

OS: Windows CE 5.0

We are using a OMAP 5910 and NOR flash which is interfaced at 0x0.

EBOOT is flashed from 0x0 to 0x20000.

On one of the HW platform we don't see that SBOOT coming up.

So, for this reason we want to load SBOOT.nb0 directly to Internal SRAM of OMAP 5910 using CCS Tools Memory Save/Load utility.

I have changed the PC to 0x20000000. But the program didn't run.

I have referred the following URL and my understanding is that it is possible to debug SBOOT or EBOOT by directly loading to memory. http://e2e.ti.com/support/embedded/wince/f/353/t/130391.aspx,

Please let me know if the procedure that I have followed is wrong.

Regards,

GSR