This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Increasing capacity of NAND on DM8168

I need to increase the capacity of the NAND flash from 1Gb to 8Gb (MT29F8G08FABWP). Can I use same wait pin from DM8168 (GPMC_WAIT0) at R/B# & R/B2# (or required to connect two different wait pins) with two nCS pin from processor at Ce# and CE2# pin of the NAND flash.  As I know, because I am using single NAND flash so wait cycle should also remains same and I should be able to use same wait signal from processor. When CE2# is selected what would be the state of R/B# at that time? Pl. guide me.