Other Parts Discussed in Thread: DM3730
Hi,all
OS:WINCE 6.0
Processor:DM3730
BSP:BSP_WINCE_ARM_A8_01_02_00
DVSDK:dvsdk_wince_01_11_00_02
When I use DVSDK-Demos\davincieffect_h264vid_mpeg1l3aud_d1ntsc_722kbps.avi
to test the DM3730 DSP, There are no image in WMP(Windows Media Player),and the debug messages are:
"
...
TIMM: ARM CPU load =6
TIMM: DSP CPU load =0
TIMM: ARM CPU load =2
TIMM: DSP CPU load =0
...
"
The DVSDK I used is dvsdk_wince_01_11_00_02. what is the reason? which drivers do relate to TI'DSP in addition to DVSDK?