This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO Not Working / Question on PinMux

Hi,

I'm trying to get a GPIO port working using both the echo commands from the shell and sysfs calls in my application but

both appear not to be toggling the actual GPIO pin on the 814x EVM.  (GPIO 29  on TestPoint TP48).

root@dm814x-evm:~# echo 29 > /sys/class/gpio/export
root@dm814x-evm:~# ls  /sys/class/gpio/gpio29
active_low  edge        subsystem   value
direction   power       uevent
root@dm814x-evm:~# echo out > /sys/class/gpio/gpio29/direction
root@dm814x-evm:~# echo 1 > /sys/class/gpio/gpio29/value
root@dm814x-evm:~# echo 0 > /sys/class/gpio/gpio29/value
root@dm814x-evm:~# cat /sys/class/gpio/gpio29/value
0
root@dm814x-evm:~# echo 1 > /sys/class/gpio/gpio29/value
root@dm814x-evm:~# cat /sys/class/gpio/gpio29/value
1

I'm reading that the cause may be that the pin mux file is not set up for this pin to be GPIO.

If this is correct....Can someone provide me support on which file this is and where it is located..as well as some direction

on how to modify this file accordingly to change a pin to a GPIO. (ie GPIO 29)....

Also...after these changes are made, does the kenel need to be rebuilt and put on SD card ?

Does the board also require pull-ups or pull-downs to make the output change ?

If there are any pins on the 814 already configured for GPIO and would work out of the box , that would also save some effort

and could test those immediately....(please identify these if available)

I would appreciate any help in getting this to work...

Thanks