Other Parts Discussed in Thread: PROFIBUS, AM1810
With respect to ProfiBus support in general and on the EVM:
#1) The ICE design is using UART1 (D15, D16) as the ProfiBus handler. Which I believe is then PR1_UART0 correct (the PRU unit's hardwired UART)?
#2) So that means it needs to be set aside as the ProfiBus pins correct?
#3) With that GPIO3_19 (C13) is being used in part of the ProfiBus control. Am I correct in assuming that this is something that would be locked in the PRU stack as well? So I need to assume it for ProfiBus?
#4) Since the ProfiBus is still being worked on its hard to look at what is going on - from what I can tell the code/stack piece items would be available by end of Q1 2012 correct? And given that any idea as to if a cost would be associated with it?
Thanks,
Bryan Busacco