The value of register 0x4800244C is 0x0C00 and based on table 1-6 chip identification, the processor is DM3730. But from the other hand The value of CONTROL_IDCODE register is 0x2B89102F and as bit 12 is “1”, it means that the processor is either AM3715 or AM3703.
Also the bit 11:10 reading is “00”, which doesn’t match with any of the values of the table 1-6.
However the assembly instruction list of the attached BOM is also confusing:
|
Assembly Instruction List |
|
|
1 |
Peel of the sticky tape on SW1 after assembly, so that user can flip switches easily |
|
2 |
This board is assembled with OMAP3730. Make sure the Assembly & Serial No. Labels read out correct Numbers. |
|
3 |
For line item #25 we have to use ES1.2 XAM3703BCBP for AM3715 build ; XDM3730BCBP should be used for 3730 builds |
By the way do you think our Mistral Eval board has the TI DSP processor DM3730? I believe the Beagleboard has it.
Thanks,
John