I wonder whether the CCS v4.2.5 supports RTDX (Real Time Data Transfer) or not. While I am importing CCS v3.1 rtdx projects into CCS v4.2.5, it shows "could not open source file, rtdx.h". Even if I set up the build options with include path, "C:\CCStudio_v3.1\C6000\rtdx\include" and with library path, "C:\CCStudio_v3.1\C6000\rtdx\lib", it shows undefined symbol "__vectors" and undefined symbol "_auto_init". Any advise is truly appreciated.
Best,
Alex