Other Parts Discussed in Thread: DM3730
Hi,all
OS: WINCE 6.0
Processor : DM3730
BSP: BSP_WINCE_ARM_A8_01_01_00_03
DVSDK: dvsdk_wince_01_11_00_02
When I use DVSDK-Demos\daviniceffect_h264vid_mpeg113aud_d1ntsc_722kbps.avi to test DM3730 DSP, There are no image in wmp(Window Media Player),and the debug
messages are :
" ...............
TIMM: ARM CPU load=6
TIMM:DSP CPU load =0
TIMM:ARM CPU load=2
TIMM:DSP CPU load=0
...............
The DVSDK I used is dvsdk_wince_01_11_00_02, which drivers do relate to DM3730 DSP in addition to DVSDK? How to solve the problem?