I'm using SDK 5.04 for AM37xx. When I run "make install" I get an error in matrix-gui_install. Here's the error:
=============================
Installing Matrix GUI
=============================
make[1]: Entering directory `/home/brad/ti-sdk-am37x-evm-05.04.00.00/example-applications/matrix-gui-2.0'
make[1]: Makefile.build: No such file or directory
make[1]: *** No rule to make target `Makefile.build'. Stop.
make[1]: Leaving directory `/home/brad/ti-sdk-am37x-evm-05.04.00.00/example-applications/matrix-gui-2.0'
make: *** [matrix-gui_install] Error 2
If I go to that directory I see that Makefile.build does not exist. What's the proper way to install matrix-gui-2.0 into the file system? If you could just give me a Makefile.build file that contains an "install" rule with the appropriate steps that would be ideal. That way I can just put that file into the matrix-gui-2.0 directory and that should fix the error.