Other Parts Discussed in Thread: OMAP3530
Hello,
I'm trying to use the OMAP3530's GPU, but I've some problems.
My final device does not have any screens, so I can't load the omaplfb module in the kernel. Here is what I've done:
First, I downloaded the Graphics_SDK_setuplinux_4_06_00_01_BinOnly.bin package, then I installed it.
Secondly, I compiled the package:
make all OMAPES=3.x BUILD=release
I got the three modules:
- bufferclass_ti.ko
- omaplfb.ko
- pvrsrvkm.ko
I successfully loaded the bufferclass_ti and the pvrsrvkm modules. But, when I try to load the omaplfb module, it does not work:
root@igep0020:~/gpu# dmesg
[ 6945.295196] omaplfb: Unknown symbol fb_blank (err 0)
[ 6945.300567] omaplfb: Unknown symbol fb_set_var (err 0)
[ 6945.317932] omaplfb: Unknown symbol registered_fb (err 0)
[ 6945.324584] omaplfb: Unknown symbol fb_pan_display (err 0)
[ 6968.406066] omaplfb: Unknown symbol fb_blank (err 0)
[ 6968.411987] omaplfb: Unknown symbol fb_set_var (err 0)
[ 6968.417388] omaplfb: Unknown symbol registered_fb (err 0)
[ 6968.423889] omaplfb: Unknown symbol fb_pan_display (err 0)
[ 6991.665283] omaplfb: Unknown symbol fb_blank (err 0)
[ 6991.671203] omaplfb: Unknown symbol fb_set_var (err 0)
[ 6991.676605] omaplfb: Unknown symbol registered_fb (err 0)
[ 6991.683135] omaplfb: Unknown symbol fb_pan_display (err 0)
How can I emulate a framebuffer on my target ?
Can I do GPGPU Programming without any framebuffer (with OpenCL for example) ?
Thanks! :)