Is there a way to evaluate the new(er) C5505A chips? The ezdsp5505 boards all appear to have the old VC5505 chips on them.
For example, from the TI store website:
The TMDX5505eZDSP is a small form factor, very low cost USB-powered DSP development tool which includes all the hardware and software needed to evaluate the industry's lowest power 16-bit DSP: TMS320VC5504 and TMS320VC5505
...and if you download the datasheet from the Mouser site, it is the VC5505 datasheet.
I need the 150MHz clock and newer features of the C5505A chip.