Other Parts Discussed in Thread: AM1808
Dear TI,
I have not seen a resolution to this post: http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/46886.aspx regarding an AM1808 SPI Port using the PRU. I looked at the latest trunk of the GForge project and don't see any SPI Port examples that I can use. The closest implementation I see is the GPIO Example. I would prefer not to invent the wheel if I don't have to. I need two SPI ports on the AM1808 but I am also using the MAC so I am down to 1 SPI perhiperal.
Sincerely,
Jason