This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How Many Streams Can DM8168 Capture?

I realize that this may be a simple question but I've been unable to find the answer.

We're considering the DM8168 for a video capture device. We'd like to be able to capture 3 1080p30 streams and encode to H.264. The literature claims that this processor supports:

-Up to 3 HD video accelerators each capable of up to 1080p60 display

But in looking at the TRM, the HDVPSS has only 2 capture devices. 

Is it possible to capture multiple streams with one capture device of the DM8168, and if so, how? We're also looking at having to capture other formats like VGA, Composite, etc. How does that change the capture? If It's not possible, is there a TI device that could be used to capture and feed the 3rd HDVICP, say thru PCIe?

All links would be appreciated.

Thanks, John