Hello,
I am trying to compile the LED example project and watch the light show on the eval board; however, my target configuration as:
Texas Instruments XDS100v2 USB Emulator/ EZDSP5535
Receives the following error:
C55xx: Error connecting to the target: (Error -600 @ 0x0) A required dynamic library could not be located. The library isn't on the search path. (Release 5.0.429.0)
I tried changing the target configuration to others but just get more errors, or it just spits out that it worked on the console but the LEDs dont change.
The SD card is still in and and is displaying "Play Aduio rom Your PC" on the display and the console for ccv4 only seems to work for:
Texas Instruments Simulator/ C55xx Rev3.0 CPU
But still changes nothing hardware wise. Is it because I have it plugged in with the mini USB? That was all that came with it, so it would be disappointing if it was.
I mean seriously, I am at the point where it would just be easier writing from assembly like I usually do on the Motorola boards. Currently working on senior design project so please help.
-Wyatt