This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel crash on USB gadget rmmod with PSP 04.06.00.07

Expert 2280 points


Hi

I'm using PSP 04.06.00.07 with new power-management features. I've rebuilt the kernel (using am335x default configuration) with just a minor change: the two musb controller are configured as host and peripheral instead of host and otg, thus modifying board-am335xevm.c as:

    .mode           = (MUSB_HOST << 4) | MUSB_PERIPHERAL,

In the EVM, when the USB peripheral port is plugged in and I execute an rmmod command of loaded USB gadget module (any of them: g_mass_storage, g_ether, g_file_storage) I get a kernel error for "Unable to handle kernel NULL pointer dereference at virtual address 0000000c". I've attached the whole error log.

Everything works fine if cable is unplugged when rmmod is executed, or if musb controllers are configured as HOST+OTG. But I need to set them as HOST+PERIP for my custom board, and the issue affects also that board so I do not think it depends on hw.

Regards,

Max




  • Hi Max,

    Our USB engineer is on travel and he may not be able to look into this issue this week. I have created a bug ticket for tracking this issue.

    https://cqweb.ext.ti.com/cqweb/main?command=GenerateMainFrame&service=CQ&schema=SDO-Web&contextid=SDOWP&entityID=SDOCM00091275&entityDefName=IncidentReport&username=readonly&password=readonly

    Thanks,

    Sekhar

  • Hi Sekhar

    Thanks for opening the ticket, in the meanwhile I've tried to debug a little bit. Please not that musb driver cause crash if built with -DDEBUG: I had to remove dev_dbg call in cppi41dma_Interrupt function. Then I've built usb musb, core and gadget with -DDEBUG.

    The composite_disconnect function is called by usb_gadget_remove_driver. But in PERIPHERAL mode case it is called a second time due to a DISCONNECT interrupt: at this time the usb_composite_dev struct associated to gadget seems to have been already cleaned, but composite_disconnect does not do any check on cdev not null, causing the crash when it calls spin_lock_irqsave(&cdev->lock, flags).

    Gadget code seems a little bit weak from this point of view, but I am not sure this is the right place to fix: something in musb driver code flow seems changed, and maybe it is not the right one. Maybe that fix would mask other potential issues. I am looking for your final patch.

    Logs follow, hope can help to understand.

    Regards

    Max

    OTG case (fine):

    root@am335x-evm:~# rmmod g_mass_storage
    [   66.481057] g_mass_storage musb-hdrc.0: unregistering UDC driver [musb-hdrc]
    [   66.488581] g cf9151a0 cdev cec3e840 cdev->config bf007b18 composite->disconnect   (null)!
    [   66.497224]  gadget: composite_disconnect gadget cf9151a0 cdev cec3e840 ...
    [   66.504494]  gadget: reset config
    [   66.507967]  gadget: unbind function 'Mass Storage Function'/cfa67ec0
    [   66.514696]  gadget: unbind
    [   66.519081] musb-hdrc musb-hdrc.0: Descriptor (8f8ac000) popped from teardown completion queue
    [   66.528145] musb-hdrc musb-hdrc.0: ep1out request cec3e9c0, 0/512 fault -104
    [   66.535500]  gadget: bulk_out_complete --> -104, 0/31
    [   66.540850]  gadget: reset interface
    [   66.544599] musb-hdrc musb-hdrc.0: ep1in: abort DMA --> 0
    [   66.550239] musb-hdrc musb-hdrc.0: ep1in
    [   66.554340] musb-hdrc musb-hdrc.0: ep1out: abort DMA --> 0
    [   66.560059] musb-hdrc musb-hdrc.0: ep1out
    [   66.570104]  lun0: close backing file
    [   66.574147]  lun1: close backing file
    [   66.578030] musb-hdrc musb-hdrc.0: START musb_gadget_stop...
    [   66.583956] musb-hdrc musb-hdrc.0: HNP: Stopping in unknown state b_peripheral
    [   66.591491] musb-hdrc musb-hdrc.0: gadget D+ pullup off
    [   66.599485] musb-hdrc musb-hdrc.0: HDRC disabled
    [   66.604300] musb-hdrc musb-hdrc.0: UNDEFINED active, deleting timer
    [   66.610851] musb-hdrc musb-hdrc.0: unregistering driver g_mass_storage
    [   66.617659] musb-hdrc musb-hdrc.0: UNDEFINED inactive, starting idle timer for 10 ms
    [   66.625759] musb-hdrc musb-hdrc.0: Poll devctl 98 (UNDEFINED)
    [   66.631753] musb-hdrc musb-hdrc.0: remove, state 1
    [   66.636770] musb-hdrc musb-hdrc.0: roothub graceful disconnect
    [   66.642871] usb usb2: USB disconnect, device number 1
    [   66.648137] usb usb2: unregistering device
    [   66.652418] usb usb2: unregistering interface 2-0:1.0
    [   66.657808] musb-hdrc musb-hdrc.0: shutdown urb cfb91340 ep1in-intr
    [   66.664467] usb usb2: usb_disable_device nuking all URBs
    [   66.672872] musb-hdrc musb-hdrc.0: HDRC disabled
    [   66.677692] musb-hdrc musb-hdrc.0: UNDEFINED inactive, starting idle timer for 10 ms
    [   66.685789] musb-hdrc musb-hdrc.0: USB bus 2 deregistered
    [   66.691461] musb-hdrc musb-hdrc.0: ... musb_gadget_stop END
    [   66.697286] musb-hdrc musb-hdrc.0: Poll devctl 98 (UNDEFINED)

    PERIPHERAL case (crash):

    root@am335x-evm:~# rmmod g_mass_storage
    [   70.707391] g_mass_storage musb-hdrc.0: unregistering UDC driver [musb-hdrc]
    [   70.714925] g cf9150b8 cdev cee20f00 cdev->config bf007b18 composite->disconnect   (null)!
    [   70.723564]  gadget: composite_disconnect gadget cf9150b8 cdev cee20f00 ...
    [   70.730828]  gadget: reset config
    [   70.734310]  gadget: unbind function 'Mass Storage Function'/cf3b30c0
    [   70.741028]  gadget: unbind
    [   70.745408] musb-hdrc musb-hdrc.0: Descriptor (8f8ac000) popped from teardown completion queue
    [   70.754475] musb-hdrc musb-hdrc.0: ep1out request ce47d900, 0/512 fault -104
    [   70.761831]  gadget: bulk_out_complete --> -104, 0/31
    [   70.767162]  gadget: reset interface
    [   70.770898] musb-hdrc musb-hdrc.0: ep1in: abort DMA --> 0
    [   70.776552] musb-hdrc musb-hdrc.0: ep1in
    [   70.780646] musb-hdrc musb-hdrc.0: ep1out: abort DMA --> 0
    [   70.786379] musb-hdrc musb-hdrc.0: ep1out
    [   70.796494]  lun0: close backing file
    [   70.800452]  lun1: close backing file
    [   70.804413] musb-hdrc musb-hdrc.0: START musb_gadget_stop...
    [   70.810348] musb-hdrc musb-hdrc.0: usbintr (20) epintr(0)
    [   70.815981] musb-hdrc musb-hdrc.0: ** IRQ peripheral usb0020 tx0000 rx0000
    [   70.823152] musb-hdrc musb-hdrc.0: <== Power=f0, DevCtl=98, int_usb=0x20
    [   70.830142] musb-hdrc musb-hdrc.0: DISCONNECT (b_peripheral) as Peripheral, devctl 98
    [   70.838309] musb g_mass_storage gadget disconnected.
    [   70.845847] musb-hdrc musb-hdrc.0: devctl 98
    [   70.850300] musb-hdrc musb-hdrc.0: musb_g_disconnect calling composite_disconnect...
    [   70.858379] g cf9150b8 cdev   (null) cdev->config 00000001 composite->disconnect 00000002!
    [   70.866999] [ERROR] composite_disconnect gadget cf9150b8 cdev   (null) : return to avoid crash!
    [   70.876114] musb-hdrc musb-hdrc.0: usbintr (1) epintr(0)
    [   70.881658] musb-hdrc musb-hdrc.0: ** IRQ peripheral usb0001 tx0000 rx0000
    [   70.888828] musb-hdrc musb-hdrc.0: <== Power=e0, DevCtl=99, int_usb=0x1
    [   70.895728] musb-hdrc musb-hdrc.0: SUSPEND (b_idle) devctl 99 power e0
    [   70.902572] musb-hdrc musb-hdrc.0: gadget D+ pullup off
    [   70.910568] musb-hdrc musb-hdrc.0: HDRC disabled
    [   70.915382] musb-hdrc musb-hdrc.0: unregistering driver g_mass_storage
    [   70.924759] musb-hdrc musb-hdrc.0: HDRC disabled
    [   70.929575] musb-hdrc musb-hdrc.0: ... musb_gadget_stop END

  • Max,

    Thanks for sharing the details. I will look into this and update sometime next week

    Ajay

  • Hi Ajay, any news on this issue? Thanks, regards.

    Max

  • I can dig up the logs if it helps you (as a working data point), but this worked fine for us on the AM335x EVM in the default PSP mode with USB0 switching g_ether.ko between g_mass_storage.ko.

    Did you defconfig the initial PSP 04.06.00.07?

    Seemed to make a big difference in USB (and other kernel) stability when I did.

  • I can dig up the logs if it helps you (as a working data point), but this worked fine for us on the AM335x EVM in the default PSP mode with USB0 switching g_ether.ko between g_mass_storage.ko.

    Do you mean you cannot reproduce the issue with AM335x EVM and PSP 04.06.00.07 original code, or even after changing the USB0 role configuration from OTG to PERIPHERAL in board-am335xevm.c file? I know everything is fine with OTG configuration, I'm facing the issue just if USB0 is configured in PERIPHERAL mode.

    Did you defconfig the initial PSP 04.06.00.07?
    Seemed to make a big difference in USB (and other kernel) stability when I did.

    What do you mean exactly with "to defconfig the initial PSP 04.06.00.07"? I've run the usual mrproper and then am335x_evm_defconfig... correct?

  • >>I'm facing the issue just if USB0 is configured in PERIPHERAL mode.

    Sorry, once we understood the default EVM config HW doc here:

    http://processors.wiki.ti.com/index.php/AM335X_USB_Driver_User_Guide_04.06.00#Port_mode_configuration

    and SW documented below, we realized we only need OTG on USB0.  Haven't tried peripheral mode.

    >> I've run the usual mrproper and then am335x_evm_defconfig... correct?

    Yup, that's it.

    A  key Linux improvement  in PSP-04.06.00.07 came from the file arch/arm/mach-omap2/board-am335xevm.c:

    static struct omap_musb_board_data musb_board_data = {
            .interface_type = MUSB_INTERFACE_ULPI,
            /*
             * mode[0:3] = USB0PORT's mode
             * mode[4:7] = USB1PORT's mode
             * AM335X beta EVM has USB0 in OTG mode and USB1 in host mode.
             */

     

  • Please use below patch which will come in next version of TI PSP release.

    ----------------------------------------------------------------------------------------------------

    diff --git a/drivers/usb/musb/musb_gadget.c b/drivers/usb/musb/musb_gadget.c
    index 305d843..47da5ed 100644
    --- a/drivers/usb/musb/musb_gadget.c
    +++ b/drivers/usb/musb/musb_gadget.c
    @@ -2120,11 +2120,6 @@ void musb_g_disconnect(struct musb *musb)
            (void) musb_gadget_vbus_draw(&musb->g, 0);

            musb->g.speed = USB_SPEED_UNKNOWN;
    -       if (musb->gadget_driver && musb->gadget_driver->disconnect) {
    -               spin_unlock(&musb->lock);
    -               musb->gadget_driver->disconnect(&musb->g);
    -               spin_lock(&musb->lock);
    -       }

            switch (musb->xceiv->state) {
            default:
    -----------------------------------------------------------------------------------------------------------------------------

    I am checking this with musb maintainer and will update if any change.

    Ajay

  • The correct fix is to use bugfix patches from latest kernel for udc_core.c as available at

    http://git.kernel.org/?p=linux/kernel/git/torvalds/linux-2.6.git;a=history;f=drivers/usb/gadget/udc-core.c;h=e5e44f8cde9a3c99052e19e5e8c641ab3123a534;hb=76e10d158efb6d4516018846f60c2ab5501900bc

    Apply below 4 patches

    usb: gadget: udc-core: fix incompatibility with dummy-hcd
    usb: gadget: udc-core: fix wrong call order
    usb: gadget: udc-core: fix asymmetric calls in remove_driver
    usb: gadget: udc-core: stop UDC on device-initiated disconnect

    Ajay

  • Hi Ajay,

    I've patched just udc_core.c as suggested, without changing musb driver code as in previously proposed patch: rmmod does not cause NULL pointer deference any longer, and everything seems working fine in HOST+PERIPHERAL modes such as in HOST+OTG modes case.

    Thanks for your support.

    Regards,

    Max