This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIE Transactions



Hello

 How  can i perform this two operations in the  DSP C6678 of Texas instrument   : 

- Generating  Configuration transactions

- Generating Memory Read from a remote device 

i have already configured one DSP C6678 as Root Complex

NB : The example given within the Device treats only memory write 

sincerely 

Younes

  • Younes,

    1. In C66x device, the PCIe remote configuration space is located starting from offset 0x2000 (i.e. 0x21802000). The RC could read/write from/to that address space to access the configuration space of remote device and the configuration transactions will be issued automatically. Please note that there is one CFG_SETUP register (offset 0x8) to be configured for different remote devices on the bus. The default values should be working to access the EP directly connected to the RC (without any PCIe switch or bridge).

    If there is PCIe switch or bridges in the system, it is better to use certain PCIe host driver on RC side to enumerate the bus and assign the bus/function/device numbers to each device on the PCIe bus.

    2. Generating memory read transaction is very similar as generating memory write transaction. The PCIe device could just read from its PCIe data space (i.e. starting from 0x60000000 for C6678 device) using EDMA or CPU read.

    Sincerely,

    Steven

  • Thank  You Steven ,

    I understood your answer , but the problem is that the remote device for me is not an other C6678 , it is a bridge function in a switch , so i want to read one register of the bridge 

    Configuration space and display the value on the console ( screen )

    Sincerely 

    Younes

  • Younes,

    I think the configuration access to bridge or switch from RC should be similar as access to EP.

    If the bus/device/function numbers of the Bridge are setup correctly in the RC CFG_SETUP register. The RC could access the configuration registers in the Bridge by reading the remote configuration space (starting from 0x21802000 in C66x PCIe).

    Or if there is BAR register in the Bridge which could be mapped to its configuration register space (similar as BAR0 mapping to C66x PCIe apps registers), the RC could generate normal memory write/read to access the Bridge registers with packet address matching to the Bridge BAR register. In this way, the RC should access to the PCIe data space (starting from 0x60000000 in C66x).

    Sincerely,

    Steven

  • Thank you Steven ,

    Actualy , i want to access a remote register which is not a PCI Express register , what i want is a function of your module C6678 , which take an adress in parameters and

    return the contain of this adress , 

    I precise :  i have the C6678 as RC , and a bridge in the other side of the link , and i want to acess to a regiser in this bridge , it is sufficient that i use your function : pcie_Readregs(.....,PCIE_LOCATION_REMOTE,...)  , while this function can  read just a PCIE register 

    NB: i specified the bus , device , function number of my bridge 

    Thanks 

  • If it is not in the PCIe configuration register space in the Bridge, I am afraid you could not use the LLD function directly.

    Another way is to do the memory read from the Bridge just as you may intend to do so. You have to configure BAR and other inbound registers in the Bridge to cover the memory location of that register you want to read from Bridge. And configure the RC outbound registers to issue the memory read to the Bridge which is just similar as normal memory read access to the remote device.

    Sincerely,

    Steven

  • Thank you Steven for your answer ,

    im trying also to perform a PIPE loopback . How to check that the loopback has been performed correctly if knowing that this kind of loopback doesnt allow looping back

    datas and allows just looping back symbols ( mentionned in the document of the C6678 of PCI express module)

    Sincerely 

    Younes 

  • Younes,

    PIPE Loopback is a test and debug feature. The Loopback master (such as a PCIe protocol tester) when connected to a device's Link (the device under the test) can place the Link and Loopback slave into the Loopback state by transmitting TS1ordered-sets with the Loopback bit asserted.

    If the C66x PCIe module is used as Loopback master, it could put the Loopback slave (at the other end of the PCIe link) into loopback mode by following the programming sequence described in the user guide. And the Loopback slave is better to be a PCIe tester which could decode and display the symbols for the user to monitor the symbols being looping back over the link.

    If C66x PCIe module is used as Loopback slave, the Loopback master is better to be a PCIe tester, which could put the Loopback slave into loopback mode and send out the symbols for testing.

    Sincerely,

    Steven

  • Hello.

    I have similar problems with PCI transactions.

    I have RC on the base C6670 and FPGA EP 

    In fact, for configuration of  memory transactions with EP, I have to configure not only remote Config Regs in 0x21802000-... space, but remote Application Regs too. For example, such as: CMD_STATUS , OB_OFFSET_INDEXn, IB_BARn, IB_OFFSETn and so.

    But.

    I can read and write remote config regs (such as remote BAR regs) in space  0x21802000-... . And I can't access Application Regs of remote EP.

    In SPRUGS6D  I am reading:

    RC can access these registers (i.e. remote Application Registers) in a PCIESS EP via the upper 1KB space of the PCIe

    configuration space.

     

    What does it mean? Is it memory range 0x21807c00-21807FFF?

    I tried to read and write that memory from my RC and not getting any good results

    With regards . Alexander

  • Hi,

    Have you run the test application on EP(FPGA) side?

    The memory space covered by BAR0 in inbound direction is completely dedicated to accessing the application registers, Address Space 0, in both RC and EP modes. It implies that the BAR0 cannot be remapped to any other location but to application registers. Any remote inbound access matching the BAR0 region will automatically be routed to these registers. It allows RC devices to control EP devices in absence of dedicated software running on EP. For RC and EP, this mapping of BAR0 to registers allows the message signaled interrupts to work. There is no support to disable BAR0 accesses from reaching the application registers.

    Take a look at similar thread:

    Thanks,

  • Sorry. But there is some problem.
    Look.
    To access application regs and data in remote EP we must enable remote BAR0 and BAR1 (which default disabled on the EP side), by writing 0x1 to 0-bit of remote BAR0_MASK and BAR1_MASK regs. For this we must allow BARn_MASK writing by seting "1" to DBI_CS2 (bit 5 in remote CMD_STATUS register). But this remote application registr is available only via EP BAR0, which is default disabled as yet while we don't enabled it .
    Vicious circle.