This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6437 with DSP/BIOS version 4.9?

Can I use DM6437 based board with DSP/BIOS version 4.9 or I have to upgrade to DSP/BIOS to 5.31.02?

  • Hi Robert Smith,

    While I don't have a CCS install with a 4.90 version of BIOS handy, I don't believe the 6437 was supported on DSP/BIOS 4.90.

    Can you check your examples directory of your BIOS 4.90 installation?  The examples should have been organized based on hardware platforms (that were supported in the release).

    For example, there's probably one for the dsk6711.  E.g.

    typical/examples/dsk6711/bios/clktest

    If there is not a "evmDM6437" directory (or similar) then this is a good indication that it really isn't supported.

    Yet another way to check is to look for the C64x+ "seed" file.  If the following file is not present, then 6437 isn't supported (since it's a C64x+ core):

    c64xxplus.cdb

    For example, you would check a directory similar to the following in the BIOS installation:

    c6000/bios/include/4.90.270/*.cdb

    Steve