This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 VPFE

DM368 VPFE has HD,VD and C_WE_FIELD pins, which can be configured as input or output.
When the device is configured embedded sync mode, can these pins configured as output and
Outputs HD,VD and Filed information corresponding to the embedded TRS instead of outputting
Internally generated sync status.