I just finished my DM6467T product, and now I need to develop a more sophisticated one using the DM8168. I'm confident the DM8168 will be able to capture four NTSC video sources using four 8-bit wide ports. But this time, instead of sending the video out one of the DaVinci video ports, I want to send it out over the (local) Ethernet. I'm not sure if the DaVinci has an "internal pathway" for doing this. Can I do this?
Also, I don't know much about video over Ethernet yet, and we're starting from an otherwise clean slate. Any recommendation on the video format over Ethernet? On the other end, we need to recreate 60fps VGA.
Note also that in parallel I'll be wanting to send video out the video ports nevertheless, using one 8-bit wide port for composite output and one 16-bit wide port for VGA output (with cheap frame rate conversion done by frame repetition). That leaves me one 8-bit port to whistle "Dixie."