This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK, Packet Accelerator conflicting with SRIO driver



hello,

Can someone please explain to me how the NDK uses the packet accelerator?  I have read the Packet Accelerator documentation and I can see how ndk applications call and initialize the PA with its necessary firmware.  However, what I don't see is how it is assigning queues and such.

I mean, what portion of the NDK configures the PA with the necessary calls that setup the engines and layers?

After I understand it better, I would also like to know if this could be causing conflicts with my SRIO driver?  I did not change anything in the Packet Accelerator initialization code in my merge, but I thought maybe the SRIO driver uses the packet accelerator too?  I saw an api about adding srio to the PA.  Please explain this API and if I should use it.

Thanks,
Brandy

PS.

C6678 EVM, mcsdk_2_00_05_17, ndk_2_20_04_26, pdk_1_0_0_17