This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does EZSDK have plan to support Composite Camera input with V4L2 interface at the DM8148 EVM ?

I have DM8148 EVM made by MISTRAL and also use EZSDK(ver. 5_03_01_15).

In order to support input for composite camera (NTSC/PAL) at EVM, I used V4L2 interface.

But EZSDK didn't have V4L2 capturing ability yet, so that I modified source to support composite camera input at the EVM,

and then I found that VPSS-v4l2.M3 firmware has a problem. VPSS-v4l2.M3 firmware didn't capture even field.

I have nothing to do any more for my project, because EZSDK has only OMX interface  for VPSS/VICP M3 firmware control interface.

My project need to support some functions like DVR/VideoPhone, so that OMX interface is not suitable to my project.

 

In these case like my project, developer need the v4l2 interface to control VPSS/VICP or any flexible interface to control VPSS/VICP.

 

 Does IT have plan for EZSDK to support Composite Camera input with V4L2 interface or any other interface at the DM8148 EVM ?