Hi,
I'm using the TMS320TCI6486 (Tomahawk) chip.
In my application I didn't implement the MDIO logic and the MDIO pins aren't connected.
I have a question regarding the TCI6486 EMAC bootloader process: when setting the boot mode to be MAC port 0 and the MACSEL pins to GMII mode, how does the chip determine the wire speed (10 Mbps / 100 Mbps / 1000 Mbps)? Is it according to the Tx and Rx input clocks? Is it possible to force a certain wire speed for the EMAC during the bootloader process?
I'd appreciate a response ASAP.
Thanks in advance,
Elad.