Other Parts Discussed in Thread: TMS320C5505
Hi,
We are using TMS320C5505, and when we try to communicatte with a LCD we can´t visualize anything in the screen. However, I can see (with a scope) in the LCD bus that the registers (LCD RD, WR, CS0, RS) and LCD(0-15) work perfectly (datasheet diagram).
I think that the problem is that we are using libraries lcd.h lcd_panel.h, that have the same functions cmdWrite and dataWrite, because we have use in our program parts of configuration from a program that was in the "evm5505_v1" and parts from a program in the "usbstk5505_v2", so it impacts in the "power on" function of the LCD.
Anyone knows if those functions are the same in both libraries (the code is not the same, but perhaps they do the same)?¿?¿ Any idea?¿
Regards,
Xabi.