This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

accessing tty drivers from User Space.



Dear All,

I have been stucked at a Point with confusion. the file /include/linux/tty.h

Has a structure name tty_struct .

I am not sure but i came across reading that . if  i have to transmit a character on the ttyS0 . then i have to use the Functions provided in the file tty_driver.h.

Following functions :

 int  (*open)(struct tty_struct * tty, struct file * filp);
 void (*close)(struct tty_struct * tty, struct file * filp);
 int  (*write)(struct tty_struct * tty,const unsigned char *buf, int count);
 void (*put_char)(struct tty_struct *tty, unsigned char ch); and many more.

m i going correct ?

If yes ....

#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <fcntl.h>
#include <sys/ioctl.h>


int main()
{
int fd=open("/dev/ttyS0",_IOC_READ);

int i = 0;

printf("=============TEST BEGIN=============\n");

if(fd == -1)
{
printf("Open File Error\n");
exit(0);                                                                         
}
else
{
printf("Open File SuccessFull=%d\n",fd);    === > fd value when i print is 3 ????
}
 

while(1)

{

//void (*put_char)(struct tty_struct *tty, unsigned char ch);

put_char(?,0x55); ===> i am stucked with this argument ..what i should pass as the first argument.

i dont know where the structure is getting updated. should i pass "tty". ?

Also it says put_char undefined ? which file i should add ?

}
printf("==============TEST END==============\n");

close(fd);
}

Please provide your views on this . i have a bit idea about the Linux.