This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which device drivers are available in the SYS/BIOS Industrial SDK for Sitara AM335x?

According to the http://www.ti.com/tool/sysbiossdk-ind-sitara the following device driver are available.

This text is copied from the above link.

Device Drivers and libraries for the Sitara ARM AM335x peripherals:

  • I2C driver
  • GPIO driver
  • UART Serial driver
  • PRUSS driver
  • SPI driver
  • NAND flash driver
  • SD/MMC driver
  • PWM driver
  • Ethernet driver

At the moment I need ethernet driver and SPI driver.
It seems to me that only EtherCat is supported in the  SYS/BIOS Industrial SDK for Sitara AM335x.

When will the rest of the device drivers be available?