This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to flash the kernel image and RFS to NAND

Other Parts Discussed in Thread: AM1808

Hi,

               I am using am1808 experimenters kit with NAND add on card. I would like to put kernel image and root file system along with UBL and U-BOOT. I am using SFH tool for flashing UBL and U-BOOT. can i use the same toool to flash kernel image and root file system in nand flash. If it is possible how can we do it.

 

Thanks

Vasu Vallabhaneni

  • Hi,

    I am using am1808 experimenters kit with NAND add on card. I would like to put kernel image and root file system along with UBL and U-BOOT. I am using SFH tool for flashing UBL and U-BOOT. can i use the same toool to flash kernel image and root file system in nand flash. If it is possible how can we do it.

    No the, serial flasher tool is only for flashing the u-boot and UBL/SPL. and not for uImage

    and filesystem. Refer this link for writing the kernel to NAND. And for filesystem, you can use

    JFFS2/YAFFS just google it you should able to get it.

    Thx,

    --Prabhakar Lad

    http://in.linkedin.com/pub/prabhakar-lad/19/92b/955