Other Parts Discussed in Thread: AM3894
Hello, I am new to the AM3894 MPU and have a question about configuring the device for Non-Multiplexed Address Data 16-Bit Device. I want to used the full address bits[27-0] in my design. I notice that a few of the GPMC address pins have dual functions. For example GMPC Address 27 is on pin AC5 or K8. Also on pin AC5 is GP0[20], and on pin K8 is GP1[9]. When I configure the device to use all 28-bits of address, which pin AC5 or K8 will address bit 27 be on?
Last, where do set the device to be in Non-Multiplexed Address Data 16-bit?
Thank you very much,
joe