Other Parts Discussed in Thread: SMJ320C25
Anyone knows if the SMJ320C26 and the SMJ320C25 shared the same die?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SMJ320C25
Anyone knows if the SMJ320C26 and the SMJ320C25 shared the same die?
Hello,
The SMJ320C26 architecture is based on the SMJ320C25 with a different internal RAM and ROM configuration. The SMJ320C26 integrates 256 words of on-chip ROM and 1568 words of on-chip RAM compared to 4K words of on-chip ROM and 544 words of on-chip RAM for the SMJ320C25. The SMJ320C26 is pin for pin compatible with the SMJ320C25.
Refer to the architecture sections of SMJ320C26 and SMJ320C25 datasheets.
However, I do not know if they share the same die.
Regards,
Mark