This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDMI output on Panda4430 for ICS



hi , I am building ICS source on Panda4430 board, it's done. I want to display output on HDMI but it's showing only black-blank screen with following log, 
it's working fine wiith DVI port.

127|shell@android:/ $ [ 3531.926818] hpd 1
[ 3531.975769] in hpd work 1, state=0
[ 3531.980316] omapdss HDMI: ENTER hdmi_display_enable
[ 3532.046661] in hpd work 2, state=1
[ 3532.701232] edid[000] = 00 ff ff ff ff ff ff 00 1c 45 30 00 01 00 00 00
[ 3532.709869] edid[010] = 18 0f 01 03 80 73 41 78 0a cf 74 a3 57 4c b0 23
[ 3532.718200] edid[020] = 09 48 4c 00 00 00 01 01 01 01 01 01 01 01 01 01
[ 3532.725372] edid[030] = 01 01 01 01 01 01 01 1d 00 72 51 d0 1e 20 6e 28
[ 3532.733825] edid[040] = 55 00 c4 8e 21 00 00 1e 01 1d 80 18 71 1c 16 20
[ 3532.741271] edid[050] = 58 2c 25 00 c4 8e 21 00 00 9e 00 00 00 fc 00 4d
[ 3532.748474] edid[060] = 53 74 61 72 20 44 65 6d 6f 00 00 20 00 00 00 fd
[ 3532.755767] edid[070] = 00 3b 3c 1f 2d 08 00 0a 20 20 20 20 20 20 01 b1
[ 3532.762939] edid[080] = 02 03 1c f2 4a 90 01 02 03 04 85 12 13 94 16 23
[ 3532.770233] edid[090] = 09 07 07 83 01 00 00 65 03 0c 00 10 00 8c 0a d0
[ 3532.779174] edid[0a0] = 8a 20 e0 2d 10 10 3e 96 00 c4 8e 21 00 00 18 8c
[ 3532.786468] edid[0b0] = 0a a0 14 51 f0 16 00 26 7c 43 00 c4 8e 21 00 00
[ 3532.793914] edid[0c0] = 98 01 1d 00 bc 52 d0 1e 20 b8 28 55 40 c4 8e 21
[ 3532.801147] edid[0d0] = 00 00 1e 01 1d 80 d0 72 1c 16 20 10 2c 25 80 c4
[ 3532.808410] edid[0e0] = 8e 21 00 00 9e 00 00 00 00 00 00 00 00 00 00 00
[ 3532.815582] edid[0f0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 e2
[ 3532.823028] edid[100] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.831573] edid[110] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.838806] edid[120] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.846099] edid[130] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.853576] edid[140] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.861907] edid[150] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.869506] edid[160] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.876892] edid[170] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.884277] edid[180] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.891479] edid[190] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.898803] edid[1a0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.906982] edid[1b0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.914245] edid[1c0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.914245] edid[1d0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.914245] edid[1e0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.914276] edid[1f0] = 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
[ 3532.914276] Division by zero in kernel.
[ 3532.914276] Backtrace:
[ 3532.914428] [<c00521a0>] (dump_backtrace+0x0/0x110) from [<c05a881c>] (dump_)
[ 3532.914428] r6:00000000 r5:df992950 r4:c07f4e70 r3:e19da000
[ 3532.914428] [<c05a8804>] (dump_stack+0x0/0x1c) from [<c00522e8>] (__div0+0x1)
[ 3532.914428] [<c00522cc>] (__div0+0x0/0x20) from [<c0215f94>] (Ldiv0+0x8/0x10)
[ 3532.914428] [<c023d1b8>] (get_detailed_timing+0x0/0x288) from [<c023e5ec>] ()
[ 3532.914428] [<c023e378>] (fb_edid_add_monspecs+0x0/0x47c) from [<c025be08>] )
[ 3532.914428] [<c025bc8c>] (hdmi_get_monspecs+0x0/0x1a0) from [<c025c450>] (hd)
[ 3532.914428] [<c025c2c4>] (hdmi_hotplug_detect_worker+0x0/0x1d0) from [<c00ae)
[ 3532.914611] [<c00adf8c>] (process_one_work+0x0/0x410) from [<c00ae744>] (wor)
[ 3532.914611] [<c00ae59c>] (worker_thread+0x0/0x490) from [<c00b5380>] (kthrea)
[ 3532.914642] [<c00b52ec>] (kthread+0x0/0x98) from [<c009b69c>] (do_exit+0x0/0)
[ 3532.914672] r7:00000013 r6:c009b69c r5:c00b52ec r4:ee375e94
[ 3532.914672] panel size 115 by 65

any one have idea how can I can connect HDMI using hdmi port.