Other Parts Discussed in Thread: AM3517, OMAP-L138
For our design we need additional Irda uarts. Therefor we added a SC16is752 to I2c.
For adding the driver I added in the drivers/serial.kconfig
config SERIAL_SC16IS752
tristate "SC16IS752 chips"
depends on I2C && GPIOLIB
select SERIAL_CORE
help
gpio driver for SC16IS752 I2C UARTs.
in drivers/serial/makefile
obj-$(CONFIG_SERIAL_SC16IS752) += sx16is752.o
in drivers/serial/serial_core.h
#define PORT_SC16IS7X2 20 /* SC16IS7x2 SPI UART */
#define PORT_MAX_8250 20 /* max port ID */
and the SC16is752.c file in the drivers/serial folder.
Then in the config of the evm am3517_evm_defconfig added 'CONFIG_SERIAL_SC16IS752=y'
If I now build the kernel I get following message:
CC drivers/serial/8250.o
CC drivers/serial/8250_early.o
make[3]: *** No rule to make target `drivers/serial/sx16is752.o', needed by `drivers/serial/built-in.o'. Stop.
make[2]: *** [drivers/serial] Error 2
make[1]: *** [drivers] Error 2
make[1]: Leaving directory `/usr/local/ti-sdk-am3517-evm/board-support/linux-2.6.37-psp04.02.00.07.sdk'
make: *** [linux] Error 2
Question now is are there more configurations to be updated to add this driver?
Regards
Marcel Stumpel