This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Severe problem on versions confliction



Hello everyone!

I'm working on OMAPL137 evm.Now I met a severe problem with the kernel. The source docunment is "Montavista-Linux-02.16.20.tar.gz".

Kernel version is "2.6.18_pro500-da830_omapl137_evm-arm_v5t_le".(use uname -r)

However, when I checked the modules, it showed as:

root@192.168.1.100:~# modprobe -l
FATAL: Could not load /lib/modules/2.6.18_pro500-da830_omapl137_evm-arm_v5t_le/m
odules.dep: No such file or directory

The directory "2.6.18_pro500-da830_omapl137_evm-arm_v5t_le" did not exist, instead it was "2.6.18_pro500-davinci_evm-arm_v5t_le". And "modules.dep" inside it was empty. 

Then I checked modules version in the /target/lib/modules/2.6.18_pro500-davinci_evm-arm_v5t_le/kernel and found their versions are all "2.6.18_pro500-davinci_evm-arm_v5t_le", different with the kernel version. Maybe this's the reason why "modprobe -l" echo errors.

The kernel version string is defined in /linux-2.6.18_pro500/localversion-mvl, 2.6.18_pro500-da830_omapl137_evm-arm_v5t_le.

I changed localversion-mvl to 2.6.18_pro500-davinci_evm-arm_v5t_le to cater for modules version and recompile the kernel.

Then I run "modprobe -l" and it displayed modules correctly. The modules.dep was correct and written with modules' infomation.

But the kenel displayed error messages of ipv6 and usb:

......

 

usbcore: disagrees about version of symbol dma_pool_create
usbcore: Unknown symbol dma_pool_create
usbcore: disagrees about version of symbol driver_attach
usbcore: Unknown symbol driver_attach
usbcore: disagrees about version of symbol device_unregister
usbcore: Unknown symbol device_unregister
usbcore: disagrees about version of symbol class_destroy
usbcore: Unknown symbol class_destroy
usbcore: disagrees about version of symbol device_initialize
usbcore: Unknown symbol device_initialize
usbcore: disagrees about version of symbol get_driver
usbcore: Unknown symbol get_driver
usbcore: disagrees about version of symbol device_for_each_child
usbcore: Unknown symbol device_for_each_child
usbcore: disagrees about version of symbol get_device
usbcore: Unknown symbol get_device
......
ipv6: Unknown symbol pneigh_enqueue
ipv6: disagrees about version of symbol sock_queue_rcv_skb
ipv6: Unknown symbol sock_queue_rcv_skb
ipv6: disagrees about version of symbol neigh_table_init
ipv6: Unknown symbol neigh_table_init
ipv6: disagrees about version of symbol skb_copy
ipv6: Unknown symbol skb_copy
ipv6: disagrees about version of symbol skb_clone
ipv6: Unknown symbol skb_clone
ipv6: disagrees about version of symbol icmp_send
ipv6: Unknown symbol icmp_send
ipv6: disagrees about version of symbol sock_release
ipv6: Unknown symbol sock_release
ipv6: disagrees about version of symbol tcp_sendpage
ipv6: Unknown symbol tcp_sendpage
......

USB can't be mounted:

So should I change the localversion_mvl and how to reconcile the version of kernel and its own modules?

In which file is the string "davinci_evm-arm_v5t_le" defined? 

I've tried to recompile modules or kenel but didnot work.

Regards