This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer0 Module clock configuration



Hi,


I'm testing the dmtimerCounter example that is provided in the Starterware 02_00_00_06 and this example works well on the EVM board evaluation module.

What I'm trying to do is to run this example with all timers available.

The problem is that I can't get through this test with both Timer 1 and 0. The DMTimer0ModuleClkConfig() and DMTimer1ModuleClkConfig() are not provided in the Starterware and I don't find the way to configure the clock module properly.

With my configuration of Timer0 clock module, the init part of the test goes well but the interrupts of Timer 0 and 1 never appear.

Here is the configuration that I use for Timer0:

void DMTimer0ModuleClkConfig(void)
{
    /* Configuring L3 Interface Clocks. */

    /* Writing to MODULEMODE field of CM_PER_L3_CLKCTRL register. */
    HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKCTRL) |=
          CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE;

    /* Waiting for MODULEMODE field to reflect the written value. */
    while(CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKCTRL) &
           CM_PER_L3_CLKCTRL_MODULEMODE));

    /* Writing to MODULEMODE field of CM_PER_L3_INSTR_CLKCTRL register. */
    HWREG(SOC_CM_PER_REGS + CM_PER_L3_INSTR_CLKCTRL) |=
          CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE;

    /* Waiting for MODULEMODE field to reflect the written value. */
    while(CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_INSTR_CLKCTRL) &
           CM_PER_L3_INSTR_CLKCTRL_MODULEMODE));

    /* Writing to CLKTRCTRL field of CM_PER_L3_CLKSTCTRL register. */
    HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) |=
          CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;

    /* Waiting for CLKTRCTRL field to reflect the written value. */
    while(CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) &
           CM_PER_L3_CLKSTCTRL_CLKTRCTRL));

    /* Writing to CLKTRCTRL field of CM_PER_OCPWP_L3_CLKSTCTRL register. */
    HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) |=
          CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP;

    /*Waiting for CLKTRCTRL field to reflect the written value. */
    while(CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) &
           CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL));

    /* Writing to CLKTRCTRL field of CM_PER_L3S_CLKSTCTRL register. */
    HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) |=
          CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP;

    /*Waiting for CLKTRCTRL field to reflect the written value. */
    while(CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) &
           CM_PER_L3S_CLKSTCTRL_CLKTRCTRL));

    /* Checking fields for necessary values.  */

    /* Waiting for IDLEST field in CM_PER_L3_CLKCTRL register to be set to 0x0. */
    while((CM_PER_L3_CLKCTRL_IDLEST_FUNC << CM_PER_L3_CLKCTRL_IDLEST_SHIFT)!=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKCTRL) &
           CM_PER_L3_CLKCTRL_IDLEST));

    /*
    ** Waiting for IDLEST field in CM_PER_L3_INSTR_CLKCTRL register to attain the
    ** desired value.
    */
    while((CM_PER_L3_INSTR_CLKCTRL_IDLEST_FUNC <<
           CM_PER_L3_INSTR_CLKCTRL_IDLEST_SHIFT)!=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_INSTR_CLKCTRL) &
           CM_PER_L3_INSTR_CLKCTRL_IDLEST));

    /*
    ** Waiting for CLKACTIVITY_L3_GCLK field in CM_PER_L3_CLKSTCTRL register to
    ** attain the desired value.
    */
    while(CM_PER_L3_CLKSTCTRL_CLKACTIVITY_L3_GCLK !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3_CLKSTCTRL) &
           CM_PER_L3_CLKSTCTRL_CLKACTIVITY_L3_GCLK));

    /*
    ** Waiting for CLKACTIVITY_OCPWP_L3_GCLK field in CM_PER_OCPWP_L3_CLKSTCTRL
    ** register to attain the desired value.
    */
    while(CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L3_GCLK !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_OCPWP_L3_CLKSTCTRL) &
           CM_PER_OCPWP_L3_CLKSTCTRL_CLKACTIVITY_OCPWP_L3_GCLK));

    /*
    ** Waiting for CLKACTIVITY_L3S_GCLK field in CM_PER_L3S_CLKSTCTRL register
    ** to attain the desired value.
    */
    while(CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_L3S_GCLK !=
          (HWREG(SOC_CM_PER_REGS + CM_PER_L3S_CLKSTCTRL) &
          CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_L3S_GCLK));


    /* Configuring registers related to Wake-Up region. */

    /* Writing to MODULEMODE field of CM_WKUP_CONTROL_CLKCTRL register. */
    HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CONTROL_CLKCTRL) |=
          CM_WKUP_CONTROL_CLKCTRL_MODULEMODE_ENABLE;

    /* Waiting for MODULEMODE field to reflect the written value. */
    while(CM_WKUP_CONTROL_CLKCTRL_MODULEMODE_ENABLE !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CONTROL_CLKCTRL) &
           CM_WKUP_CONTROL_CLKCTRL_MODULEMODE));

    /* Writing to CLKTRCTRL field of CM_PER_L3S_CLKSTCTRL register. */
    HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CLKSTCTRL) |=
          CM_WKUP_CLKSTCTRL_CLKTRCTRL_SW_WKUP;

    /*Waiting for CLKTRCTRL field to reflect the written value. */
    while(CM_WKUP_CLKSTCTRL_CLKTRCTRL_SW_WKUP !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CLKSTCTRL) &
           CM_WKUP_CLKSTCTRL_CLKTRCTRL));

    /* Writing to CLKTRCTRL field of CM_L3_AON_CLKSTCTRL register. */
    HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CM_L3_AON_CLKSTCTRL) |=
          CM_WKUP_CM_L3_AON_CLKSTCTRL_CLKTRCTRL_SW_WKUP;

    /*Waiting for CLKTRCTRL field to reflect the written value. */
    while(CM_WKUP_CM_L3_AON_CLKSTCTRL_CLKTRCTRL_SW_WKUP !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CM_L3_AON_CLKSTCTRL) &
           CM_WKUP_CM_L3_AON_CLKSTCTRL_CLKTRCTRL));

    /* Writing to MODULEMODE field of CM_WKUP_TIMER0_CLKCTRL register. */
    HWREG(SOC_CM_WKUP_REGS + CM_WKUP_TIMER0_CLKCTRL) |=
          CM_WKUP_TIMER0_CLKCTRL_MODULEMODE_ENABLE;

    /* Waiting for MODULEMODE field to reflect the written value. */
    while(CM_WKUP_TIMER0_CLKCTRL_MODULEMODE_ENABLE !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_TIMER0_CLKCTRL) &
           CM_WKUP_TIMER0_CLKCTRL_MODULEMODE));

    /* Verifying if the other bits are set to required settings. */

    /*
    ** Waiting for IDLEST field in CM_WKUP_CONTROL_CLKCTRL register to attain
    ** desired value.
    */
    while((CM_WKUP_CONTROL_CLKCTRL_IDLEST_FUNC <<
           CM_WKUP_CONTROL_CLKCTRL_IDLEST_SHIFT) !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CONTROL_CLKCTRL) &
           CM_WKUP_CONTROL_CLKCTRL_IDLEST));

    /*
    ** Waiting for CLKACTIVITY_L3_AON_GCLK field in CM_L3_AON_CLKSTCTRL
    ** register to attain desired value.
    */
    while(CM_WKUP_CM_L3_AON_CLKSTCTRL_CLKACTIVITY_L3_AON_GCLK !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CM_L3_AON_CLKSTCTRL) &
           CM_WKUP_CM_L3_AON_CLKSTCTRL_CLKACTIVITY_L3_AON_GCLK));

    /*
    ** Waiting for IDLEST field in CM_WKUP_L4WKUP_CLKCTRL register to attain
    ** desired value.
    */
    while((CM_WKUP_L4WKUP_CLKCTRL_IDLEST_FUNC <<
           CM_WKUP_L4WKUP_CLKCTRL_IDLEST_SHIFT) !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_L4WKUP_CLKCTRL) &
           CM_WKUP_L4WKUP_CLKCTRL_IDLEST));

    /*
    ** Waiting for CLKACTIVITY_L4_WKUP_GCLK field in CM_WKUP_CLKSTCTRL register
    ** to attain desired value.
    */
    while(CM_WKUP_CLKSTCTRL_CLKACTIVITY_L4_WKUP_GCLK !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CLKSTCTRL) &
           CM_WKUP_CLKSTCTRL_CLKACTIVITY_L4_WKUP_GCLK));

    /*
    ** Waiting for CLKACTIVITY_L4_WKUP_AON_GCLK field in CM_L4_WKUP_AON_CLKSTCTRL
    ** register to attain desired value.
    */
    while(CM_WKUP_CM_L4_WKUP_AON_CLKSTCTRL_CLKACTIVITY_L4_WKUP_AON_GCLK !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CM_L4_WKUP_AON_CLKSTCTRL) &
           CM_WKUP_CM_L4_WKUP_AON_CLKSTCTRL_CLKACTIVITY_L4_WKUP_AON_GCLK));

    /*
    ** Waiting for CLKACTIVITY_TIMER0_GFCLK field in CM_WKUP_CLKSTCTRL
    ** register to attain desired value.
    */
    while(CM_WKUP_CLKSTCTRL_CLKACTIVITY_TIMER0_GCLK !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_CLKSTCTRL) &
                  CM_WKUP_CLKSTCTRL_CLKACTIVITY_TIMER0_GCLK));

    /*
    ** Waiting for IDLEST field in CM_WKUP_TIMER0_CLKCTRL register to attain
    ** desired value.
    */
    while((CM_WKUP_TIMER0_CLKCTRL_IDLEST_FUNC <<
           CM_WKUP_TIMER0_CLKCTRL_IDLEST_SHIFT) !=
          (HWREG(SOC_CM_WKUP_REGS + CM_WKUP_TIMER0_CLKCTRL) &
           CM_WKUP_TIMER0_CLKCTRL_IDLEST));

}

  • Hi Frederic

    In AM335x there are 8 instances of timers(DMTimer0 - DMTimer7). Amongst these DMTimer0 is a secure timer and DMTimer1(DMTimer1_1ms) is used as a 1ms timer. Other timers are having the basic functionality(DMTimer 2-7).

    There is no support given for DMTimer1_1ms in StarterWare(i.e. there is no Device abstraction layer(DAL) for DMTimer_1ms) and one cannot use the same DMTimer example application in StarterWare for this instance(IP is different). If you want to use this Timer you could refer the function "void initializeTimer1(void)" from demoTimer.c file of StarterWare demo example(DMTimer_1ms is used in demo app).

    Also, DMTimer0 instance is used as a secure timer and what i could find regarding this is, clock to drive DMTimer0 can be got from 4 places(32KHz RC Osc, CLK_32KHz from PRCM, Master Oscillator 24MHz, TCLKIN) and to program this a register is given whose description is below

    Maybe you could try for different clock configurations from the above table. Hope this helps.

     

    Regards

    Jeethan