Other Parts Discussed in Thread: AM1808
Hi,
I am working with AM1808 based custom made board where we don't have ethernet. So i thought of loading the kernel image and rfs through serial port. I used the following commands in uboot.
loadb 0xc0700000
nand erase 0x200000 0x300000
nand write.i 0xC0700000 0x200000 0x300000
setenv bootcmd 'nand read.e 0xc1180000 0x500000 0x500000; nboot.e 0xc0700000 0 0x200000; bootm'
here i am loading the kernel image to RAM and i copied the same to NAND address 200000. but my uboot is giving an error message as follows
NAND read: device 0 offset 0x500000, size 0x500000
5242880 bytes read: OK
Loading from nand0, offset 0x200000
Image Name: Linux-2.6.37N6
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1984924 Bytes = 1.9 MiB
Load Address: c0008000
Entry Point: c0008000
## Booting kernel from Legacy Image at c0700000 ...
Bad Header Checksum
ERROR: can't get kernel image!
Please suggest me a solution for this.
Thanks
Vasu Vallabhaneni
0xc0700000
nand erase 0x200000 0x300000
nand write.i 0xC0700000 0x200000 0x300000
setenv bootcmd 'nand read.e 0xc1180000 0x500000 0x500000; nboot.e 0xc0700000 0 0x200000; bootm'