Dear TI,
I have been researching using Quad SPI flash on my design with AM335x but would like have the option to boot from it. From what I am reading in the technical reference manual: http://www.ti.com/lit/ug/spruh73d/spruh73d.pdf and on this forum post: http://e2e.ti.com/support/dsp/sitara_arm174_microprocessors/f/791/t/168471.aspx it appears that there are working examples for UBoot as well as Starterware for a SPI Nor Flash off of SPI0.
It looks like in order to use the Quad SPI Flash I would need to connect it not to SPI0 but to the MMC controller pins. Has anyone demonstrated using the raw boot mode of the MMC/SD perhiperal to boot off a Quad SPI Flash? Or perhaps there is a better way to utilize a quad SPI flash?
Sincerely,
Jason