Our board which uses DM3730 has LS-Research wireless module(Ti-Wifi 1271) and vendor we are working with says
that in order to operate this module in the AP mode we probably better start using Linux kernel 3.x.
On the hand we depend on TI DVSDK's codecs server package for (video encode/decode) and dsplink Linux kernel driver which we think
right now works on the Linux kernel 2.6.37.
Here is our questions:
1. Is it true that LS-Research wireless module(Ti-Wifi 1271) can be used in the AP mode only with kernels 3.x?
If yes, then what extra functionality is missing in the the 2.6.37 Linux kernel?
2. Does TI plan to support codecs server package and dsplink driver on Linux kernel versions 3.x?
If yes then when?
3. We know that there is the SysLink product which in some way is the successor of the DspLink.
Does SysLink package support DM3730?
Does TI plan to release DVSDK and codecs server package for the SysLink or we better stick
with the latest TI DVSDK which currently uses DspLink given the fact that we want to release
our product in a year from the spring of 2012?
4. Are we doing the right thing while trying to use 2.6.37 kernel version instead of 3.x? (May be TI's drivers for all the peripherals
of the DM3730 are already included into the Linux kernel 3.x source tree?)
Are there any benefits when using Linux kernel 2.6.37 (OMAPPSP_04.02.00.07) from TI for the DM3730?
Thank you