Hello,
I am using OMAPL138 USB0 as device only mode.
When I was designed target board, the user guide(SPRUfm9d) had been described that USB0_ID should pull-up to DVDD33 rail with an external 10K ohm resistor.
But, I have noticed the description is changed in current TRM(SPRUh77a).
SPRUh77a
(P1593) 35.2.2 Signal Descriptions
USB0_ID : For OTG mode or device only mode of operation, do NOT connect the USB0_ID pin, that is, leave the pin floating.
Since I have already produced equipments, could you give me some advices?
- We must change USB0_ID pin as floating?
(Now, our equipment have been operate properly.)
- Can you disclose why the handling has been changed?
Best regards,
RY