This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sofware running at a very low speed in the EZDSP C5515

Hello,

We have a C5515 EVM board and an EZDSP C5515 board.  The same software that runs at a normal speed in the C5515 board when loaded in the EZDSP runs at a much lower speed.  What could be causing this to happen?  Is there anything that needs to be done in the EZDSP to run at a normal speed?

When the sample software that came with the Code Composer for the EZDSP is loaded it also seems to run much slower than the original software that came alredy loaded in the EZDSP.

Thank you.

Regards,

 

Eduardo