This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368IPNC image tearing issue

Hi all,

In DM368IPNC-imx036 board I am facing image tearing issue in the D1 resolution

of H.264/MPEG4.If we enable the VS/VNF/LDC algorithm then there is no Image tearing issue.

In function DRV_imgsCalcFrameTime in the file drv_imgsCalcCfg_IMX036_3MP the default

setting is as follows:

pModeCfg->vdint0        =     512;     // <--- modify this parameter and check the crop condition in all streams.
pModeCfg->vdint1        =     0;        //800;
pModeCfg->vdint2        =     IMGS_H_MAX-1;

 If we change this default setting to

  pModeCfg->vdint0        = 10;    //10;    //1023;    //(5); //512an
  pModeCfg->vdint1        = 800;        //800;
  pModeCfg->vdint2        = IMGS_H_MAX-1;

then there is no Image tearing issue in None mode but Image tearing issue is coming in Video stabilization mode.

If i can have the right values so that there is no Image tearing issue in any of the modes.

Thanks and Regards,

Mayank