This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 PCIe Root Complex Boot

Hello.

In my application C6678 device configured on POR like Root Complex. Can this DSP be able to boot from EP, if it configured as Root Complex?

  • Igor,

    How do you plan to configure the C6678 as RC on POR?

    If you use a memory boot mode to boot the C6678 into RC on PCIe, then that same memory-based secondary boot code can leave the C6678 waiting for a third boot process from an EP device.

    There is no native boot process to get directly into the mode you describe.

    Regards,
    RandyP