This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure OMAP-L137 DSP EDMA interrupt

Other Parts Discussed in Thread: OMAP-L137

Hi, I'm working on a project  with the platform of OMAP-L137 ,But while I configure the intertupts of DSP I have some  problem, In our project ,we use EDMA for the SPI development,,and after each time the EDMA finish,   an  interrupt routing should be executed .But how can i configure the interrupt,Would this be ringht?
*(volatile int *)REGA_DRAE0=0xFFFFFFFF;  //assign  the EDMA channal to region 0
*(volatile int *)REGA_DRAE1=0xFFFFFFFF; //assign  the EDMA channal to region 1
*(volatile int *)REGA_INTMUX3=(12<<0)+(13<<8)+(14<<16)+(15<<24);//select the events for interruput
IER|=(1<<INTSOURCE_EDMA);//enable the interrupt

in fact, I'm quite confused about which ID of event is corresponding to the interrupt of EDMA,and which interrupt shouid be enabled?