I am able to generate a secure boot image and boot custom C5505 hardware using TI's program to transfer the secure boot image via USB.
I have written a program to do this. I can transfer the secure boot image to the USB bulk endpoint on the 5505. Is there a trick to getting the usb to boot after the image is transferred. This question has been asked before on the forum, but the answer was not posted.
Do you have sample C source on how to transfer the secure boot image to the 5505 viat the USB?