This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please check a summary of DM36x timer registers availability.

Hi Champs,

I made the summary below, mentioned in this subject, because I could not find any documentation that summarize the register information.
So, could you please check it against the device spec whether it's correct or not?

 Offset | Acronym      | Timer 0 | Timer 1 | Timer 2 | Timer 3 | Timer 4
--------+--------------+---------+---------+---------+---------+---------
  00h   | PID12        |    X    |    X    |    X    |    X    |    X
  04h   | EMUMGT       |    X    |    X    |    X    |    X    |    X
  10h   | TIM12        |    X    |    X    |    X    |    X    |    X
  14h   | TIM34        |    X    |    X    |    X    |    X    |    X
  18h   | PRD12        |    X    |    X    |    X    |    X    |    X
  1Ch   | PRD34        |    X    |    X    |    X    |    X    |    X
  20h   | TCR          |    X    |    X    |    X    |    X    |    X
  24h   | TGCR         |    X    |    X    |    X    |    X    |    X
  28h   | WDTCR        |    -    |    -    |    X    |    -    |    -
  34h   | REL12        |    X    |    X    |    -    |    X    |    X
  38h   | REL34        |    X    |    X    |    -    |    X    |    X
  3Ch   | CAP12        |    -    |    -    |    -    |    X    |    -
  40h   | CAP34        |    -    |    -    |    -    |    X    |    -
  44h   | INTCTL_STAT  |    -    |    -    |    -    |    X    |    -

Thanks in advance for your cooperation.

Best regards,
j-breeze