This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Supported data rate for turbo decoder of c6416T

Hi 

Please confirm that the TCP core of C6416 dsp can output 3.2Mbps data.

  • Please reply !!!

    The datasheet says that it can carry 7 , 2 Mbps channels. 

    Does that mean it can carry 1, 6 Mbps channel.

    Also can any one explains this 2 Mbps is the input to the turbo decoder or is it the output.

    Waitin for response