This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to configure the drivers' parameters for DM648??



Hi. I'm using DM648 to capture  video(its format is 1080p25 that is the width is 1920 pixel,and the height is 1080 lines) from FPGA. The video is YCbCr422(Y-8bits,Cb,Cr-4bits),so we use the video port 0(16pins) as input. The pspdriver-version  is pspdriver_1_10_00_09. However, I find this driver doesn't support this format. So, How   to configure the drivers' parameters?  thank you!

     M.Y. Wu